Part Number: TIDM-1000
Tool/software: Code Composer Studio
Hi Sir
We followed the Reference Design of TIDM-1000 to estimate Vienna PFC performance.There are questions below:
1. When build level set to 1~3,Could the EVM run in 208VL-L 1.2KW and 400VL-L 2.4KW?
2. Whatever build level is in 1~4,the EVM must run in CCS debug mode.
Could the EVM run automatically after code is programed? If yes,How to do?
Best regards,
Harry