This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: "Failed to generate all binary outputs."

Part Number: TMS320F28377S
Other Parts Discussed in Thread: TI-CGT

Greetings to all,

Greetings to all,

I am implementing FOC for PMSM drive in real time setup with f28377s processor and generating code using embedded coder MATLAB2017a for the processor... I couldn't complete the building process since the error report says that it was "Failed to generate all binary outputs. Anyone please help me to solve this issue asap. I have attached Diagnostic viewer report for the reference.

Thanks

Best Regards

Priya

=== Build (Elapsed: 1:02 min) ===
    ### Starting build procedure for model: closed_loop
    ### Generating code into build folder: E:\Matlab_Workspace\closed_loop_ert_rtw
    Warning:Use fixed buffer size in 'closed_loop/PLL/Model/Automatic Gain Control/Fundamental (PLL-Driven)/Mean (Variable Frequency)1/Model/Variable Transport Delay' is not selected. When generating GRT/ERT code, Simulink will automatically use fixed buffer of the initial buffer size set by user. Code generation results and simulation results may differ
    Warning:Use fixed buffer size in 'closed_loop/PLL/Model/Automatic Gain Control/Fundamental (PLL-Driven)/Mean (Variable Frequency)2/Model/Variable Transport Delay' is not selected. When generating GRT/ERT code, Simulink will automatically use fixed buffer of the initial buffer size set by user. Code generation results and simulation results may differ
    Warning:Use fixed buffer size in 'closed_loop/PLL/Model/Mean (Variable Frequency)/Model/Variable Transport Delay' is not selected. When generating GRT/ERT code, Simulink will automatically use fixed buffer of the initial buffer size set by user. Code generation results and simulation results may differ
    ### Invoking Target Language Compiler on closed_loop.rtw
    ### Using System Target File: C:\Matlab R2017a Installation files\rtw\c\ert\ert.tlc
    ### Loading TLC function libraries
    Warning:  The data type "int8" uses a word size that is not available on the intended target.
        Fixed-point signals using this data type will be put inside a larger word or multi words.  When used,
    extra software will be generated to force this larger word or multi words to emulate a smaller
    word.  This emulation is helpful when your prototype target and your final
    production target are not the same.  If the smaller word size does NOT exist
    on the final production target, then consider increasing the word size to
    one that is supported.
    Warning:  The data type "uint8" uses a word size that is not available on the intended target.
    .
    Warning:  The data type "boolean" uses a word size that is not available on the intended target.
    .
    ### Initial pass through model to cache user defined code
    ### Caching model source code
    ...............................................................................
    .......................................................
    ### Writing source file closed_loop.c
    ### Writing header file closed_loop_private.h
    ### Writing header file closed_loop.h
    ### Writing header file closed_loop_types.h
    ### Writing header file rtwtypes.h
    ### Writing header file zero_crossing_types.h
    .
    ### Writing header file rtGetInf.h
    ### Writing source file rtGetInf.c
    ### Writing header file rt_defines.h
    ### Writing header file rt_nonfinite.h
    ### Writing source file rt_nonfinite.c
    .
    ### Writing header file rtGetNaN.h
    ### Writing source file rtGetNaN.c
    ### Writing source file closed_loop_data.c
    ### Writing header file rtmodel.h
    ### Writing source file ert_main.c
    ### TLC code generation complete.
    .### Evaluating PostCodeGenCommand specified in the model
    ### Creating CCS Project at : E:\Matlab_Workspace\closed_loop_ert_rtw\CCS_Project
    ### CCS project created successfully Open project in Code Composer Studio.
    ### Using toolchain: Texas Instruments C2000 Code Generation Tools v6.0.0 | gmake (64-bit Windows)
    ### 'E:\Matlab_Workspace\closed_loop_ert_rtw\closed_loop.mk' is up to date
    ### Building 'closed_loop': "C:\MATLAB~2\bin\win64\gmake"  -B -f closed_loop.mk all
     
    E:\Matlab_Workspace\closed_loop_ert_rtw>cd .  
     
    E:\Matlab_Workspace\closed_loop_ert_rtw>if "" == "" ("C:\MATLAB~2\bin\win64\gmake"  -B -f closed_loop.mk all )  else ("C:\MATLAB~2\bin\win64\gmake"  -B -f closed_loop.mk  )  
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=MW_c28xx_board.obj MW_c28xx_board.c 
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=rt_backsubrr_dbl.obj rt_backsubrr_dbl.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=rt_forwardsubrr_dbl.obj rt_forwardsubrr_dbl.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=rt_lu_real.obj rt_lu_real.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=rt_matrixlib_dbl.obj rt_matrixlib_dbl.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=MW_c28xx_csl.obj MW_c28xx_csl.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=MW_c28xx_pwm.obj MW_c28xx_pwm.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=closed_loop.obj closed_loop.c
    "C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include/stdbool.h", line 36: warning: incompatible redefinition of macro "false" (declared at line 22 of "rtwtypes.h")
    "C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include/stdbool.h", line 37: warning: incompatible redefinition of macro "true" (declared at line 26 of "rtwtypes.h")
    "closed_loop.c", line 414: warning: argument of type "int_T *" is incompatible with parameter of type "int32_T *"
    "closed_loop.c", line 425: warning: argument of type "int_T *" is incompatible with parameter of type "const int32_T *"
    "closed_loop.c", line 470: warning: argument of type "int_T *" is incompatible with parameter of type "const int32_T *"
    "closed_loop.c", line 524: warning: argument of type "int_T *" is incompatible with parameter of type "const int32_T *"
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=closed_loop_data.obj closed_loop_data.c
    "C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include/stdbool.h", line 36: warning: incompatible redefinition of macro "false" (declared at line 22 of "rtwtypes.h")
    "C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include/stdbool.h", line 37: warning: incompatible redefinition of macro "true" (declared at line 26 of "rtwtypes.h")
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=rtGetInf.obj rtGetInf.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=rtGetNaN.obj rtGetNaN.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=rt_nonfinite.obj rt_nonfinite.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=c2837xSBoard_Realtime_Support.obj C:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src/c2837xSBoard_Realtime_Support.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=F2837xS_CpuTimers.obj C:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/source/F2837xS_CpuTimers.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=F2837xS_DefaultISR.obj C:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/source/F2837xS_DefaultISR.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=F2837xS_GlobalVariableDefs.obj C:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/source/F2837xS_GlobalVariableDefs.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=F2837xS_PieCtrl.obj C:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/source/F2837xS_PieCtrl.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=F2837xS_PieVect.obj C:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/source/F2837xS_PieVect.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=F2837xS_SysCtrl.obj C:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/source/F2837xS_SysCtrl.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 -s -v28 -ml --float_support=fpu32 --output_file=F2837xS_usDelay.obj C:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/source/F2837xS_usDelay.asm
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 -s -v28 -ml --float_support=fpu32 --output_file=F2837xS_CodeStartBranch.obj C:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/source/F2837xS_CodeStartBranch.asm
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=F2837xS_Dma.obj C:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/source/F2837xS_Dma.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=F2837xS_Adc.obj C:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/source/F2837xS_Adc.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=F2837xS_Gpio.obj C:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/source/F2837xS_Gpio.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=profiler_Support.obj C:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src/profiler_Support.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=c2837xSSchedulerTimer0.obj C:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src/c2837xSSchedulerTimer0.c
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include" -v28 --float_support=fpu32 -ml -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=1 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=16 -DCPU1 -DF2837X_REG_FORMAT -DMW_F2837XS -DSTACK_SIZE=512 -DRT -DMODEL=closed_loop -DNUMST=2 -DNCSTATES=15 -DHAVESTDIO -IE:/Matlab_Workspace -IC:/MATLAB~2/simulink/include/sf_runtime -IE:/Matlab_Workspace/closed_loop_ert_rtw -IC:/MATLAB~2/extern/include -IC:/MATLAB~2/simulink/include -IC:/MATLAB~2/rtw/c/src -IC:/MATLAB~2/rtw/c/src/ext_mode/common -IC:/MATLAB~2/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/inc -IC:/MATLAB~2/toolbox/shared/can/src/scanutil -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~3/include -IC:/CCSV7I~1/CONTRO~1/DEVICE~1/F2837xS/v191/F2837X~1 -IC:/MATLAB~2/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/shared/externalmode_daemon/include --output_file=ert_main.obj ert_main.c
    "C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include/stdbool.h", line 36: warning: incompatible redefinition of macro "false" (declared at line 22 of "rtwtypes.h")
    "C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/include/stdbool.h", line 37: warning: incompatible redefinition of macro "true" (declared at line 26 of "rtwtypes.h")
    "### Creating standalone executable "../closed_loop.out" ..." 
    C:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/bin/cl2000 -z -IC:/CCSV7I~1/ccsv7/tools/compiler/TI-CGT~4.LTS/lib --stack_size=512 --warn_sections --heap_size=1024 --reread_libs --rom_model -m"closed_loop.map" -l"rts2800_fpu32.lib" --define BOOT_FROM_FLASH=0 --define BOOT_USING_BL=0 --output_file=../closed_loop.out MW_c28xx_board.obj rt_backsubrr_dbl.obj rt_forwardsubrr_dbl.obj rt_lu_real.obj rt_matrixlib_dbl.obj MW_c28xx_csl.obj MW_c28xx_pwm.obj closed_loop.obj closed_loop_data.obj rtGetInf.obj rtGetNaN.obj rt_nonfinite.obj c2837xSBoard_Realtime_Support.obj F2837xS_CpuTimers.obj F2837xS_DefaultISR.obj F2837xS_GlobalVariableDefs.obj F2837xS_PieCtrl.obj F2837xS_PieVect.obj F2837xS_SysCtrl.obj F2837xS_usDelay.obj F2837xS_CodeStartBranch.obj F2837xS_Dma.obj F2837xS_Adc.obj F2837xS_Gpio.obj profiler_Support.obj c2837xSSchedulerTimer0.obj ert_main.obj C:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/rtlib/IQmath_fpu32.lib C:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src/c2837xSPeripherals.cmd C:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src/c28377S.cmd   
    <Linking>
    warning: build attribute vendor section TI missing in
       "C:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackag
       es/tic2000/rtlib/IQmath_fpu32.lib<IQ29cosPU.obj>": compatibility cannot be
       determined
    warning: build attribute vendor section TI missing in
       "C:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackag
       es/tic2000/rtlib/IQmath_fpu32.lib<IQ29mpyI32int.obj>": compatibility cannot
       be determined
    warning: build attribute vendor section TI missing in
       "C:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackag
       es/tic2000/rtlib/IQmath_fpu32.lib<IQ29sinPU.obj>": compatibility cannot be
       determined
    warning: build attribute vendor section TI missing in
       "C:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackag
       es/tic2000/rtlib/IQmath_fpu32.lib<IQmathTables.obj>": compatibility cannot
       be determined
    "C:/ProgramData/MATLAB/SupportPackages/R2017a_1/toolbox/target/supportpackages/tic2000/src/c28377S.cmd", line 107: error:
       program will not fit into available memory.  run placement with
       alignment/blocking fails for section ".ebss" size 0x247f2 page 1.  Available
       memory ranges:
       RAMLS_DATA   size: 0x1000       unused: 0xccd        max hole: 0xccd
       RAMD1        size: 0x800        unused: 0x800        max hole: 0x800
       RAMGS_DATA   size: 0x8000       unused: 0x8000       max hole: 0x8000
    error: errors encountered during linking; "../closed_loop.out" not built
    >> Compilation failure
    gmake: *** [../closed_loop.out] Error 1
    E:\Matlab_Workspace\closed_loop_ert_rtw>echo The make command returned an error of 2
    The make command returned an error of 2
    E:\Matlab_Workspace\closed_loop_ert_rtw>An_error_occurred_during_the_call_to_make
    'An_error_occurred_during_the_call_to_make' is not recognized as an internal or external command,
    operable program or batch file.
    ### Creating HTML report file closed_loop_codegen_rpt.html
    ### Build procedure for model: 'closed_loop' aborted due to an error.
    Error:Error(s) encountered while building "closed_loop":
    ### Failed to generate all binary outputs.