Part Number: TMS320F28377S
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
I wanted to ask a very basic question on CAN implementation. Since I am totally a beginner in this, I am not sure about the implementation.
I have two TMS320F28377S Launchpads with me. How can I connect these two for establishing CAN communication between these two. It is just for checking basic programs. What will be the simplest method for connecting these two. What would be the simplest thing I can use as CAN bus. Would the terminating resistors be needed since I'll be placing them really close. Do I actually need to use twisted pair cables or can I use just two wires to connect CAN_H and CAN_L of two Launchpads together. It is not for any real application but for learning purpose for the time-being. I may use it for real application later but not for now. I need to check whether I am receiving the data I am sending correctly and also whether I am receiving positive acknowledgement.
Could anyone please suggest the easiest and simplest method to achieve this?
PS: Correct me if I have mentioned anything wrong above since I am a beginner.