Part Number: TMS320F28377D
Other Parts Discussed in Thread: OPA320
Hello
We are developing a BLDC board.
To do this, we use the 28377 controller.
We use the ADC to get the DCLink voltage (about 24VDC) and then the motor phase current (U and V).
The DCLink voltage is divided by resistor ( divisor = 21).
The Phase current is getting by a shunt resistor of 8mohms and then amplificator.
An extract of the scheme is provided.
The current measure is Ok.
The DCLink voltage is Ok.
But now, we control the motor. All run correctly.
Now, on a speed Loop control, we asked null speed. Then motor not turn, but a torque is applied. Then when we try to move the motor with the hand, the measured motor current increase proportinally to the torque applied.
Until now, all it is Ok!
But on this state (Motor speed = 0 with an hand applied torque), the ADC measure done on the channel affected to the DCLink increase whereas ADC input stay stable! Then the software get about 30V whereas the input represent 24V!
The current in phase motor is 4A. This correspond to the ADC get value.
It is like the ADC input of the Motor phase current affect the measured value on the channel for the DCLink voltage!
I check all other voltage (GND, VRef HI, Vref Low etc..) All physical voltage is Ok.
Just the register AdccResultRegs.ADCRESULT1 increase from #1390 to about #1500...#1600 !
The Analog input of the DCLink is 1.13V, this correspond to the 24V of the DCLink. #1500..#1600 should say this input is about 25..26V.
This error increase with motor current. When motor current is about 10A, the Measure DCLink up to 30V whereas Physical DClink voltage stay to 24V...
Schema:
This is the Init code :
/* *********************************/
/* Resolver Fbk - sine *//* NOTE!!! ADCINC2 not used on this board, linked to GND */
/* *********************************/
AdccRegs.ADCSOC0CTL.bit.CHSEL = 2; /* Configure the Pin associated to the Adc/SOC */
AdccRegs.ADCSOC0CTL.bit.ACQPS = 30; /* sample window in SYSCLK cycles (ACQPS + 1) x 200MHz ^-1 = 155ns (Datasheet min = 75ns) */
AdccRegs.ADCSOC0CTL.bit.TRIGSEL = 15; /* PWM6 SocA => 160KHz */ /* Selection on which event Soc will trig the start of conversion */
/* ***************************************/
/* Bus Voltage Feedback */
/* ***************************************/
AdccRegs.ADCSOC1CTL.bit.CHSEL = 3; /* Configure the Pin associated to the Adc/SOC */
AdccRegs.ADCSOC1CTL.bit.ACQPS = 30; /* sample window in SYSCLK cycles (ACQPS + 1) x 200MHz ^-1 = 155ns (Datasheet min = 75ns) */
AdccRegs.ADCSOC1CTL.bit.TRIGSEL = 5; /* PWM1 SocA => 10KHz *//* Selection on which event Soc will trig the start of conversion */
/* ****************************/
/* Shunt motor current V */
/* *********************************/
AdcdRegs.ADCSOC0CTL.bit.CHSEL = 3; /* Configure the Pin associated to the Adc/SOC */
AdcdRegs.ADCSOC0CTL.bit.ACQPS = 30; /* sample window in SYSCLK cycles (ACQPS + 1) x 200MHz ^-1 = 155ns (Datasheet min = 75ns) */
AdcdRegs.ADCSOC0CTL.bit.TRIGSEL = 5; /* PWM1 SocA => 10KHz *//* Selection on which event Soc will trig the start of conversion */
/* Configure PPB to eliminate subtraction related calculation */
AdcdRegs.ADCPPB1CONFIG.bit.CONFIG = 0; /* PPB is associated with SOC0 */
AdcdRegs.ADCPPB1CONFIG.bit.OFFCAL = 0; /* Write zero to this for now till offset ISR is run */
What could be the cause of the "ADC dependence"?