This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28374S: Two parameters decide how code works

Part Number: TMS320F28374S

Tool/software: TI C/C++ Compiler

Hi,

Customer is using CCS V6 and compiler V15 for an application.

They found that, with or without two specific parameters, code can or can't work.

Will you tell me how to identify the issue? This is the second time happened.

In details,

1) With two parameters as below, the code works well;

2) Without these two parameters, the code can't work well.

Here attached the two different maps.

Thanks a lot.https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/171/map.7z

Br, Jordan