Part Number: TMS320F280049
Other Parts Discussed in Thread: AMC1100
Hi, TI engineers,
I am using the PGA4 inside F280049 to be an amplifier for detecting outside diferential voltage purpose.
At first, I left the PGA4_GND pin disconnected while sent about 1.1V to PGA4_IN (C3 pin, actually), and then found badly noise output from PGA4_OUT, and measured about 800mV at PGA4_GND pin.
Then I tried to connect the PGA4_GND pin to VSSA directly and got a stable and constant ADC resault from PGA4_OUT internally.
So it seems that PGA4_GND is more like an output pin and should be grounded. Here comes the problem: what if a voltage different from 800mV (maybe 1000mV or 600mV) is sent to PGA4_GND to be the negative signal of diferential volatage? Actually, I chose AMC1100 to the external differential voltage input for F280049, its VOUTN is about 1000mV in our application, can it connect to PGA4_GND directly? And should they grounded, too?
Best regards.