Tool/software: Code Composer Studio
Hello,
We create a Project in one PC (CCS Version 6.1.1.00022) and we are trying to make it compile in another PC (importing the first project to CCS Version 6.1.0.00104). The problem is that only in this second PC, there are several headers that can’t be found.
When we open Project Properties -> C2000 Compilers -> Include Options, there are some missing paths that do exist in Project Propertis of the first PC.
If we add those missing paths to the project and we compare resulting .cproject files there is a difference, the path is added in one more section of .cproject file.
Why is that? Can we work with the project in these 2 versions of CCS?
Thank you very much.
Paloma