This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28065: long branch and older instruction

Part Number: TMS320F28065

HI everybody , 

I need in my code to do a jump ( from app to boot ) .

 one option is to use this  JUMP to APPLICATION ( I found in the past in some app note and you can see in my PS  ) .

it is working , but I am scared maybe will not work in future due to compiler settings/cahnges  etc . 

questions : do you reccomend it or  better a long branch ? 

any suggestion/idea ?

thank you 

regards

Carlo

PS here us the code 

 

//-------  DECLARATIONS ----------------------------

static pFunction      JumpToApplication;

typedef void (*pFunction)(void);

//----------------------------------------------------------

 

[…]

 

692         JumpToApplication = (pFunction) (ulStartAddress/2);

               ESTOP0:

3f4fe1:   2901        CLRC         SXM

3f4fe2:   761F02DC    MOVW         DP, #0x2dc

3f4fe4:   0660        MOVL         ACC, *-SP[32]

3f4fe5:   FF40        SFR          ACC, 1

3f4fe6:   1E2A        MOVL         @0x2a, ACC

 

694         JumpToApplication();

 

3f4fe7:   FF69        SPM          #0

3f4fe8:   C52A        MOVL       XAR7, @0x2a

3f4fe9:   3E67        LCR          *XAR7

695     }