This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320LF2407A: Can't Initialize Target CPU. Error 0X00000A00/-1144, Error During OCS. Timeout."

Part Number: TMS320LF2407A

Hi, 

I am trying to flash QainQin TMS320LF2407 EVM with the EPP5100 Emulator, once after importing the configuration from the CCS setup, it display  "Can't Initialize Target CPU. Error 0X00000A00/-1144, Error During OCS. Timeout."

But with the same Emulator configuration, when i connect spectrum digital TMS320LF2407EVM, I can successfully load the configuration and launch the CCS2.20.

Could any one help me in this regards.

Thanks 

Ayyappan.A