Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: LMR62421
Hi,
I want to supply an external device with 5V from the LAUNCHXL-28379D. According to the documentation I can disconnect jumpers J1-3 to isolate the board from USB, and supply 3.3V externally. The internal step-up regulator will supply the 5V rail if I connect JP6.
What is the maximum current which can be drawn from this 5V supply? According to the datasheet of the LMR62421 it should be up to 2.1A? This seems quite high, will this work without overheating?
Regards,
Killian