Part Number: DRV8312-C2-KIT
Other Parts Discussed in Thread: DRV8312
Hello,
I am working with DRV8312EVM RevD along with Anaheim motor BLY172S-24V-4000. I want to create an accurate plant model for the same in MATLAB. I searched in the datasheet and found that the MOSFET Rds_on is 80 mOhm. Also the R_shunt is 10 mOhm and R_tot_shunt is 5 mOhm. In wanted to know the overall board resistance for the DRV8312EVM board which I need to consider apart from the motor resistance while the motor is spinning.