Part Number: TMS320F28377D
Team,
When I use HRPWM to drive full bridge, I need to sync 2 PWMs. However, sync signal is generated on system clock, not high-resolution edge. when I need to change the PWM frequency often, for example once in a 8 period, due to sync signal is not generated on high-resolution edge, there should be timing error on 2nd PWM module.
PWM frequency is changing between 700kHz~900kHz. How should I make perfect sync in this situation?
Regards,
Ted