Other Parts Discussed in Thread: MOTORWARE, DRV8312
Hello,
I need to drive a motor with this board. The problem is that I need the driver to change the speed periodically: let's say start at 2000 rpm for 100 ms, go up to 3000 rpm for 100 ms (with a ramp of 50 ms), and then go back to 2000 rpm.
I've been trying to change the example code (BLDC_Sensorless.c), but I can't understand anything. Is there any guide which explains how the programming was done? Because the comments and other pdfs aren't explanatory at all. Or else, can anyone guide me through the changes I need to make?
Thank you very much,
Federico