This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSSOLARUINVKIT with



Hi, 

I'm using TMDSSOLARUINVKIT. 

My question is: why it is not possible to transfer power from the inverter to the AC source.

I would have preferred to remove the resistance and leave the connection betwin the inverter and the ac source.

Thanks in advance for any help.

Reama

  • Reama,

    If you have a good quality four quadrant AC source which can sink in current like the grid you can remove the resistance. Typical AC sources are not four quadrant and cannot sink in power. 

    However, please note at that point you are testing the board , under conditions where it has not been tested before.

    regards

    Manish Bhardwaj