Part Number: TMDSECATCNCD379D
Other Parts Discussed in Thread: CONTROLSUITE, TMS320F28379D, TLK110
Tool/software: Code Composer Studio
When I debug the TMDSECATCNCD379D, encounter 3 questions ,as belows:
1、TMDSETHERCATCNCD379D project choose option 2 which is _F2837xD_CCARD_EFMIF_RAM. then build project, press run->load program and run program.
BOX1 had been scaned in TwinCAT3.1 .When setup advanced settings to write eeprom, it always hints no responding and can display nothing like figures shown. What am i doing wrong?
2. I want to choose the project option 1 flash or 2 ram ASYN16 .But another problem comes out. When I press dubug button, windows form appear to give a session"load program error".
of course, CCS give another 3 warning under the problwm window. I don not know how to fix it .
My CCS is Version: 8.0.0.00016 .
3、From spruig9,Page20 shows that program eeprom need to choose ESI ,this means choosingTMDSECATCNCD379D EtherCAT slave (ASYNC16) .xml.
SPRUIF9 P19 No.3 show that Write eeprom then to choose pdi_test_app_emif.bin.
so which one is correct to write eeprom?