This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/DRV8301-69M-KIT: CCS/DRV8301-69M KIT lab-10e starting delay on motor run

Part Number: DRV8301-69M-KIT


Tool/software: Code Composer Studio

Hello, I faced with a problem that lab10e-flying start delays at startup even i try to run the motor right after enabling the system. After approximately 3-4 seconds motor starts running in set speed. My friend suggested that program may be performing some calibrations at start up that preventing motor to run at the beginning. I took a look but couldnot find such calibration work or any other thing to cause delay and few weeks passed without solution because i had to work on someother stuff so any suggestions where should i look to prevent time delay?