I want the following Steps to read the data:
But I am sending address twice which I dont want:
Here is my scope image:
Code Snippet is follows:
I2caRegs.I2CMDR.bit.IRS = 1; // reset I2C // Make sure I2C is not busy and has stopped while (I2caRegs.I2CSTR.bit.BB == 1); // busy loop I2caRegs.I2CSTR.bit.SCD = 1; // Clear the SCD bit (stop condition bit) while(I2caRegs.I2CMDR.bit.STP == 1); // stop bit loop I2caRegs.I2CSAR.all = 0x00; // I2C slave address I2caRegs.I2CCNT = 1; // assume register address is one byte while (I2caRegs.I2CSTR.bit.BB == 1); // still busy? //I2caRegs.I2CMDR.all = 0x2620; // start, no stop bit, master, tx, reset I2C 00100110 I2caRegs.I2CMDR.bit.NACKMOD = 0; // NACK mode bit I2caRegs.I2CMDR.bit.FREE = 0; // Stop I2C when suspended I2caRegs.I2CMDR.bit.STT = 1; // START condition bit I2caRegs.I2CMDR.bit.STP = 0; // STOP condition bit I2caRegs.I2CMDR.bit.MST = 1; // Master mode I2caRegs.I2CMDR.bit.TRX = 1; // Transmitter mode I2caRegs.I2CMDR.bit.XA = 0; // 7-bit addressing mode I2caRegs.I2CMDR.bit.RM = 0; // Nonrepeat mode I2caRegs.I2CMDR.bit.DLB = 0; // Digital loopback mode is disabled I2caRegs.I2CMDR.bit.IRS = 1; // The I2C module is enabled I2caRegs.I2CMDR.bit.STB = 0; // The I2C module is not in the START byte mode I2caRegs.I2CMDR.bit.FDF = 0; // Free data format mode is disabled I2caRegs.I2CMDR.bit.BC = 0; // 8 bits per data byte while(I2caRegs.I2CSTR.bit.XRDY == 0); // Do nothing till bus is free I2caRegs.I2CDXR.all = 0x01; // register address of the sensor (1 byte) while(!I2caRegs.I2CSTR.bit.ARDY); // all ready? //I2caRegs.I2CMDR.all = 0x2C20; // start, stop bit when CNT =0, master, rx, reset I2C 00101100 I2caRegs.I2CMDR.bit.NACKMOD = 0; // NACK mode bit I2caRegs.I2CMDR.bit.FREE = 0; // Stop I2C when suspended I2caRegs.I2CMDR.bit.STT = 1; // START condition bit I2caRegs.I2CMDR.bit.STP = 1; // STOP condition bit I2caRegs.I2CMDR.bit.MST = 1; // Master mode I2caRegs.I2CMDR.bit.TRX = 0; // Receiver mode I2caRegs.I2CMDR.bit.XA = 0; // 7-bit addressing mode I2caRegs.I2CMDR.bit.RM = 0; // Nonrepeat mode I2caRegs.I2CMDR.bit.DLB = 0; // Digital loopback mode is disabled I2caRegs.I2CMDR.bit.IRS = 1; // The I2C module is enabled I2caRegs.I2CMDR.bit.STB = 0; // The I2C module is not in the START byte mode I2caRegs.I2CMDR.bit.FDF = 0; // Free data format mode is disabled I2caRegs.I2CMDR.bit.BC = 0; // 8 bits per data byte I2caRegs.I2CCNT = 1; // only read one byte data if(I2caRegs.I2CSTR.bit.NACK == 1) { I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT; // 0x0002 } I2caRegs.I2CMDR.bit.STP = 1; // stop bit when CNT=0 while(!I2caRegs.I2CSTR.bit.SCD); // stop bit detected? data[0] = I2caRegs.I2CDRR.all; // read one byte data
So if possible is there a way where I can just write 8 bits and then just become master receiver without sending address?
Thanks
Sagar