Part Number: DRV8312-C2-KIT
There are two bundle of wires coming out of the Nema Size 17 BLDC Motor. A bundle of three wires are connected to MOA, MOB, MOC on the DRV8312EVM board. There are another bundle of 5 wires, what connections to the board are to be made for these 5 wires?
Completely new to TI microprocessors and InstaSpin solutions. Could use all the help, possible, links, clues as where to begin etc.
Thanks,
ps. its also first time I've posted on a professional forum, so I apologize if I break any rules here that I'm unaware of.