Part Number: TMS320F28335
I have a question about the eCAN module (SPRUEU1).
The document says at pag. 45:
"The following bits are set regardless of the corresponding interrupt masks in the CANGIM register: MTOFn, WDIFn, BOIFn, AAIFn (...)"
If so, whats the purpose of the bits MTOM, WDIM, BOIM, AAIM (...) in the CANGIM reg ??
On the page 76 those bits are represented as switches for MTOF0/1, WDIF0/1, BOIF0/1, AAIF0/1 (...) in a contradictory way, in my view, with what was said in the quoted paragraph !
Or:MTOFn is not MTOF0 / MTOF1; WDIFn is not WDIF0 / MDIF1; BOIFn is not BOIF0 / BOIF1; and so on...? If not, what are those bits, because I couldnt find them in any register... just MTOF0, MTOF1, BOIF0, BOIF1 (...) at CANGIF0 and CANGIF1 register.
Thanks