This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: 28035 SPI does not work properly with 7bit mode

Part Number: TMS320F28035

Hi TI team,

I have been struggling with SPI configuration for PICCOLO 28035 device. 

I used the sample code for SPI loopback without interrupt which worked fine. I disabled the loopback and connected the SIMO and SOMI pins together. 

This also worked just fine. 

Then I changed the character size to 8 bits instead of 16. I did not see any data on SIMO line for nearly 3sec. At the same time, clock and CS/STEA was working just fine. 

My code is as below. Can you please let me know what is the issue?

include "DSP28x_Project.h" // Device Headerfile and Examples Include File

// Prototype statements for functions found within this file.
void spi_xmit(Uint16 a);
void spi_fifo_init(void);
void spi_init(void);
void error(void);

void main(void)
{
Uint16 sdata; // send data
Uint16 rdata; // received data

// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2803x_SysCtrl.c file.
InitSysCtrl();

// Step 2. Initialize GPIO:
// This example function is found in the DSP2803x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio(); // Skipped for this example
// Setup only the GP I/O only for SPI-A functionality
// This function is found in DSP2803x_Spi.c
InitSpiaGpio();

// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;

// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2803x_PieCtrl.c file.
InitPieCtrl();

// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;

// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in DSP2803x_DefaultIsr.c.
// This function is found in DSP2803x_PieVect.c.
InitPieVectTable();

// Step 4. Initialize all the Device Peripherals:
spi_fifo_init(); // Initialize the Spi FIFO
spi_init(); // init SPI

// Step 5. User specific code:
// Interrupts are not used in this example.
sdata = 0x0000;
for(;;)
{
// Transmit data
spi_xmit(sdata);
// Wait until data is received
while(SpiaRegs.SPIFFRX.bit.RXFFST !=1) { }
// Check against sent data
rdata = SpiaRegs.SPIRXBUF;
if(rdata != sdata) error();
sdata++;

DELAY_US(10000);
}
}

// Step 7. Insert all local Interrupt Service Routines (ISRs) and functions here:

void error(void)
{
__asm(" ESTOP0"); // Test failed!! Stop!
for (;;);
}

void spi_init()
{
SpiaRegs.SPICCR.all =0x0007; // Reset on, rising edge, 8-bit char bits
SpiaRegs.SPICTL.all =0x0006; // Enable master mode, normal phase,
// enable talk, and SPI int disabled.
SpiaRegs.SPIBRR =0x007F;
SpiaRegs.SPICCR.all =0x0087; // Relinquish SPI from Reset, no loop back
SpiaRegs.SPIPRI.bit.FREE = 1; // Set so breakpoints don't disturb xmission
}

void spi_xmit(Uint16 a)
{
SpiaRegs.SPITXBUF=a;
}

void spi_fifo_init()
{
// Initialize SPI FIFO registers
SpiaRegs.SPIFFTX.all=0xE040;
SpiaRegs.SPIFFRX.all=0x2044;
SpiaRegs.SPIFFCT.all=0x0;
}