This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: Error 0x80000200/-1047 Fatal Error during: OCS

Part Number: TMS320F28335


Hi guys

I had a sudden shut down in my PC while my board F28335 was connected to the USB port. After that, I can't work with my DSP board at all and CCS 3.3 doesn't recognize the board. I receive the following error:

Error connecting to the target:
Error 0x80000200/-1047
Fatal Error during: OCS,
PTI_ERR_EMU_CLOSE Error Occured at 0x00000000


I/O Port = 0

Board Name: F28335 XDS100 USB Emulator
Cpu Name: TMS320C2800_0

Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.

The other problem in the board is that the board is overheated. Is there any hope that it works again or I should replace the board? In the case that it can't be repaired, I should replace the micro *** or whole DSP evolution board (Experimenter Kit)?

Kind Regards,

Abolfazl.