This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: Can CLB support pulse train input from PLC

Part Number: TMS320F280049

Hi Champs,

My customer is designing 2 axis servo using one F280049, no FPGA/CPLD. And servo motor's position sensor is optical encoder, which used QEP to get the position. F280049 has 2 QEPs, and who will be used to decode the position sensor. 

The position input from PLC is pulse train input, which can be decoded by QEP. There are 6 types from their spec, and you can see the pulse type as follows.

And additional 2 QEP are needed. So is it possible to use CLB to decode the pulse train commend?

Thanks.

Regards,

Young