This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: Problem with McBSP-B

Part Number: TMS320F28335
Other Parts Discussed in Thread: C2000WARE, ADS7809

Hello,

I am using a 16bit ADC input to the McBSP-B, receive serial data MDRB on GPIO25, receive clock MCLKRB on GPIO60 and receive frame synch MFSRB on GPIO61.

My problem is the Receiver ready bit RRDY is not set and data in not loaded into Data Receive Register DRR1.

If the Transmit frame-synchronization polarity bit FSRP is toggled with the emulator at run time, I get good data in DRR1, it is like the receive frame-sync signal MFSRB is not starting a transfer.

The oscope CH1 is MFSRB, CH2 is MCLKRB and CH3 is MDRB. When I read the GPIO inputs with the emulator all signals are correct.

void InitMcbspb(void)

{

// McBSP-B register settings

McbspbRegs.SPCR2.all=0x0000; // Reset FS generator, sample rate generator & transmitter
McbspbRegs.SPCR1.all=0x0000; // Reset Receiver, Right justify word
// McbspbRegs.SPCR1.bit.DLB = 1; // Enable loopback mode for test. Comment out for normal McBSP transfer mode.

McbspbRegs.MFFINT.all=0x0; // Disable all interrupts

McbspbRegs.RCR2.all=0x0; // Single-phase frame, 1 word/frame, No companding (Receive)
McbspbRegs.RCR1.all=0x0;

McbspbRegs.XCR2.all=0x0; // Single-phase frame, 1 word/frame, No companding (Transmit)
McbspbRegs.XCR1.all=0x0;

McbspbRegs.PCR.bit.FSXM = 1; // FSX generated internally, FSR derived from an external source

McbspbRegs.SRGR2.bit.CLKSM = 1; // CLKSM=1 (If SCLKME=0, i/p clock to SRG is LSPCLK)
McbspbRegs.SRGR2.bit.FPER = 31; // FPER = 32 CLKG periods

McbspbRegs.SRGR1.bit.FWID = 0; // Frame Width = 1 CLKG period
McbspbRegs.SRGR1.bit.CLKGDV = CLKGDV_VAL; // CLKG frequency = LSPCLK/(CLKGDV+1)

delay_loop(); // Wait at least 2 SRG clock cycles

InitMcbspb16bit(); // 16-bit word

McbspbRegs.PCR.bit.FSRP = 1; // Frame-synchronization pulse FSR is active low.
McbspbRegs.PCR.bit.CLKRP = 1; // Receive data sampled on rising edge of MCLKR

McbspbRegs.PCR.bit.CLKXM = 1; // CLKX generated internally, CLKR derived from an external source
delay_loop(); // Wait at least 2 SRG clock cycles
McbspbRegs.SPCR2.bit.GRST=1; // Enable the sample rate generator
clkg_delay_loop(); // Wait at least 2 CLKG cycles
McbspbRegs.SPCR2.bit.XRST=1; // Release TX from Reset
McbspbRegs.SPCR1.bit.RRST=1; // Release RX from Reset
McbspbRegs.SPCR2.bit.FRST=1; // Frame Sync Generator reset

}

void InitMcbspa16bit(void)
{
McbspaRegs.RCR1.bit.RWDLEN1=2; // 16-bit word
McbspaRegs.XCR1.bit.XWDLEN1=2; // 16-bit word
}

void InitMcbspbGpio(void)
{
EALLOW;
/* Configure McBSP-A pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be McBSP functional pins.
// Comment out other unwanted lines.

//GpioCtrlRegs.GPAMUX1.bit.GPIO12 = 3; // GPIO12 is MDXB pin (Comment as needed)
// GpioCtrlRegs.GPAMUX2.bit.GPIO24 = 3; // GPIO24 is MDXB pin (Comment as needed)
//GpioCtrlRegs.GPAMUX1.bit.GPIO13 = 3; // GPIO13 is MDRB pin (Comment as needed)
GpioCtrlRegs.GPAMUX2.bit.GPIO25 = 3; // GPIO25 is MDRB pin (Comment as needed)
//GpioCtrlRegs.GPAMUX1.bit.GPIO14 = 3; // GPIO14 is MCLKXB pin (Comment as needed)
// GpioCtrlRegs.GPAMUX2.bit.GPIO26 = 3; // GPIO26 is MCLKXB pin (Comment as needed)
// GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 3; // GPIO3 is MCLKRB pin (Comment as needed)
GpioCtrlRegs.GPBMUX2.bit.GPIO60 = 1; // GPIO60 is MCLKRB pin (Comment as needed)
//GpioCtrlRegs.GPAMUX1.bit.GPIO15 = 3; // GPIO15 is MFSXB pin (Comment as needed)
// GpioCtrlRegs.GPAMUX2.bit.GPIO27 = 3; // GPIO27 is MFSXB pin (Comment as needed)
// GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 3; // GPIO1 is MFSRB pin (Comment as needed)
GpioCtrlRegs.GPBMUX2.bit.GPIO61 = 1; // GPIO61 is MFSRB pin (Comment as needed)

/* Enable internal pull-up for the selected pins */
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
// GpioCtrlRegs.GPAPUD.bit.GPIO24 = 0; // Enable pull-up on GPIO24 (MDXB) (Comment as needed)
//GpioCtrlRegs.GPAPUD.bit.GPIO12 = 0; // Enable pull-up on GPIO12 (MDXB) (Comment as needed)
//GpioCtrlRegs.GPAPUD.bit.GPIO25 = 0; // Enable pull-up on GPIO25 (MDRB) (Comment as needed)
//GpioCtrlRegs.GPAPUD.bit.GPIO13 = 0; // Enable pull-up on GPIO13 (MDRB) (Comment as needed)
//GpioCtrlRegs.GPAPUD.bit.GPIO26 = 0; // Enable pull-up on GPIO26 (MCLKXB) (Comment as needed)
//GpioCtrlRegs.GPAPUD.bit.GPIO14 = 0; // Enable pull-up on GPIO14 (MCLKXB) (Comment as needed)
// GpioCtrlRegs.GPAPUD.bit.GPIO3 = 0; // Enable pull-up on GPIO3 (MCLKRB) (Comment as needed)
//GpioCtrlRegs.GPBPUD.bit.GPIO60 = 0; // Enable pull-up on GPIO60 (MCLKRB) (Comment as needed)
// GpioCtrlRegs.GPAPUD.bit.GPIO27 = 0; // Enable pull-up on GPIO27 (MFSXB) (Comment as needed)
//GpioCtrlRegs.GPAPUD.bit.GPIO15 = 0; // Enable pull-up on GPIO15 (MFSXB) (Comment as needed)
// GpioCtrlRegs.GPAPUD.bit.GPIO1 = 0; // Enable pull-up on GPIO1 (MFSRB) (Comment as needed)
//GpioCtrlRegs.GPBPUD.bit.GPIO61 = 0; // Enable pull-up on GPIO61 (MFSRB) (Comment as needed)


/* Set qualification for selected input pins to asynch only */
// This will select asynch (no qualification) for the selected pins.
// Comment out other unwanted lines.
GpioCtrlRegs.GPAQSEL2.bit.GPIO25 = 3; // Asynch input GPIO25 (MDRB) (Comment as needed)
//GpioCtrlRegs.GPAQSEL1.bit.GPIO13 = 3; // Asynch input GPIO13 (MDRB) (Comment as needed)
// GpioCtrlRegs.GPAQSEL2.bit.GPIO26 = 3; // Asynch input GPIO26(MCLKXB) (Comment as needed)
//GpioCtrlRegs.GPAQSEL1.bit.GPIO14 = 3; // Asynch input GPIO14 (MCLKXB) (Comment as needed)
// GpioCtrlRegs.GPAQSEL1.bit.GPIO3 = 3; // Asynch input GPIO3 (MCLKRB) (Comment as needed)
GpioCtrlRegs.GPBQSEL2.bit.GPIO60 = 3; // Asynch input GPIO60 (MCLKRB) (Comment as needed)
// GpioCtrlRegs.GPAQSEL2.bit.GPIO27 = 3; // Asynch input GPIO27 (MFSXB) (Comment as needed)
//GpioCtrlRegs.GPAQSEL1.bit.GPIO15 = 3; // Asynch input GPIO15 (MFSXB) (Comment as needed)
// GpioCtrlRegs.GPAQSEL1.bit.GPIO1 = 3; // Asynch input GPIO1 (MFSRB) (Comment as needed)
GpioCtrlRegs.GPBQSEL2.bit.GPIO61 = 3; // Asynch input GPIO61 (MFSRB) (Comment as needed)


EDIS;
}

void InitXintf32Gpio()
{
EALLOW;
GpioCtrlRegs.GPBMUX2.bit.GPIO48 = 3; // XD31
GpioCtrlRegs.GPBMUX2.bit.GPIO49 = 3; // XD30
GpioCtrlRegs.GPBMUX2.bit.GPIO50 = 3; // XD29
GpioCtrlRegs.GPBMUX2.bit.GPIO51 = 3; // XD28
GpioCtrlRegs.GPBMUX2.bit.GPIO52 = 3; // XD27
GpioCtrlRegs.GPBMUX2.bit.GPIO53 = 3; // XD26
GpioCtrlRegs.GPBMUX2.bit.GPIO54 = 3; // XD25
GpioCtrlRegs.GPBMUX2.bit.GPIO55 = 3; // XD24
GpioCtrlRegs.GPBMUX2.bit.GPIO56 = 3; // XD23
GpioCtrlRegs.GPBMUX2.bit.GPIO57 = 3; // XD22
GpioCtrlRegs.GPBMUX2.bit.GPIO58 = 3; // XD21
GpioCtrlRegs.GPBMUX2.bit.GPIO59 = 3; // XD20
// GpioCtrlRegs.GPBMUX2.bit.GPIO60 = 3; // XD19
// GpioCtrlRegs.GPBMUX2.bit.GPIO61 = 3; // XD18
GpioCtrlRegs.GPBMUX2.bit.GPIO62 = 3; // XD17
GpioCtrlRegs.GPBMUX2.bit.GPIO63 = 3; // XD16

GpioCtrlRegs.GPBQSEL2.bit.GPIO48 = 3; // XD31 asynchronous input
GpioCtrlRegs.GPBQSEL2.bit.GPIO49 = 3; // XD30 asynchronous input
GpioCtrlRegs.GPBQSEL2.bit.GPIO50 = 3; // XD29 asynchronous input
GpioCtrlRegs.GPBQSEL2.bit.GPIO51 = 3; // XD28 asynchronous input
GpioCtrlRegs.GPBQSEL2.bit.GPIO52 = 3; // XD27 asynchronous input
GpioCtrlRegs.GPBQSEL2.bit.GPIO53 = 3; // XD26 asynchronous input
GpioCtrlRegs.GPBQSEL2.bit.GPIO54 = 3; // XD25 asynchronous input
GpioCtrlRegs.GPBQSEL2.bit.GPIO55 = 3; // XD24 asynchronous input
GpioCtrlRegs.GPBQSEL2.bit.GPIO56 = 3; // XD23 asynchronous input
GpioCtrlRegs.GPBQSEL2.bit.GPIO57 = 3; // XD22 asynchronous input
GpioCtrlRegs.GPBQSEL2.bit.GPIO58 = 3; // XD21 asynchronous input
GpioCtrlRegs.GPBQSEL2.bit.GPIO59 = 3; // XD20 asynchronous input
// GpioCtrlRegs.GPBQSEL2.bit.GPIO60 = 3; // XD19 asynchronous input
// GpioCtrlRegs.GPBQSEL2.bit.GPIO61 = 3; // XD18 asynchronous input
GpioCtrlRegs.GPBQSEL2.bit.GPIO62 = 3; // XD17 asynchronous input
GpioCtrlRegs.GPBQSEL2.bit.GPIO63 = 3; // XD16 asynchronous input

InitXintf16Gpio();
}

Any help is help is appreciated,

Curtis Randall

  • Curtis,

    A few comments.
    First, the housekeeping: Please use the Code context import in the rich text editor if you plan to post code again in the future. This helps keep the thread more readable, as the C syntax is highlighted properly.

    With that, on to the content. Please address these questions so I can better assist:
    1. What is the external ADC you are communicating with? It appears that you intend to use ClockStop Mode (SPI mode) of the McBSP, is this correct? If so, your configuration and HW setup is incorrect. Refer to the SPI Operation Using Clock Stop Mode section of the User's guide as well as the McBSP SPI mode example in c2000Ware.
    2. Do you intend to have the digital loopback bit enabled?
    3. Toggling FSRP is not a valid use case in any mode of operation. This is a configuration/control bit, modifying this while the McBSP receiver is out of reset (RRST = 1), could lead to undefined behavior. I understand you were doing this as a debug step, but even then it is generally not recommended.

    I hope this gets you started.

    Thanks,
    Mark
  • Hello Mark,

    I will use rich text in the future.

    1. The external ADC is a ADS7809 or equivalent, we have several sources. Yes I intended SPI mode. I copied then modified Example_2833xMcBSP_DLB.c. Next I will look at Example_2833xMcBSP_SPI_DLB.c.

    2. I did not intent to have digital loopback bit enabled, is this the problem?

    3. I understand toggling FSRP is not recommended, just noticed it read the data.

    Thank you,

    Curtis Randall

  • Hello Mark,

    Using MCLKXB and MFSXB as inputs and reprogramming as McBSP SPI Slave worked.

    Thanks,

    Curtis Randall