Tool/software: Code Composer Studio
Hello,
I encountered the following errors while building a project. The nature of the error is one but i have it in 5 different places of my code. I am struggling to understand why i am getting this error.
Description Resource Path Location Type
#66 expected a ";" main_c28.c PC3_c28revA line 1344 C/C++ Problem
Below is the code fragment where i encounter the errors
CLR_SS;
//Set the data(1)/command(0) flag
if(DATA==destination)
{
SET_MOSI; // Error 1 line here
}
else
{
CLR_MOSI; // Error 2 line here
}
//Clock it in.
CLR_SCK;
SET_SCK;
//Clear the read(1)/write(0) flag to write, clock it in.
CLR_MOSI; // Error 3 line here
//Clock it in.
CLR_SCK;
SET_SCK;
for(mask=0x80;mask;mask>>=1)
{
if(mask&command) {
SET_MOSI; // Error 4 line here
}
else {
CLR_MOSI; // Error 5 line here
}
CLR_SCK;
SET_SCK;
}
//Release the chip and end SPI Transfer
SET_SS;
I have indicated the lines where i receive the error above. I clearly terminate the statement, yet the compiler says " expected a ";" ".
As always, appreciate any help.
Thanks,
Srini