This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

more recent OS for TMS320F280X = DSP/BIOS?

Hello,

I need to update the OS on a F2808, and it appears that the neither SYS/BIOS or RTOS support this chip, and that the latest OS that is supported is DSP/BIOS 5.42.  Can you confirm that this is correct?

Regards,

Robert

  • Hi Robert,

    It is supported in SYS/BIOS. Take a look in the "Supported Devices" in the release notes of SYS/BIOS.

    Or at the examples in Resource Explorer (showing Classic here from CCS 7.4).

    Note: I'd use SYS/BIOS instead of TI-RTOS for C2000. TI-RTOS for C2000 only includes examples for the Concerto devices. It also includes OS aware drivers for the M3 side of the Concerto devices, but not the C28 side. The SYS/BIOS product has examples (as shown above) for all the supported devices. You can get SYS/BIOS from here: 

    Todd

  • Thanks. Will go SYS-BIOS.

    Robert