This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SEED-DEC2812

RESPECTED SIR/MADAM,

                                                     I  KIRAN  STUDYING MTECH AND I PRESENTLY DOING PROJECT ON BLDC MOTOR AND THE PROBLEM IS WHEN THE CODE FOR SEED-DEC2812(DSP TMS320LF2812). THE HEADER FILES  FOR SEED-DEC2812(DSP TMS320LF2812)  ARE NOT WORKING PROPERLY MEANS  SOME REGISTERS ARE NOT WORKING AND CANNOT CORRECTLY MAPPED

LIKE THIS

IMR        .set        0004h
IFR        .set        0006h
SCSR1        .set        7018h
SCSR2        .set        7019h

        SO,PLEASE PROVIDE HEADER FILES FOR SEED -DEC2812(DSP TMS320LF2812)

  • ki ravikiran said:

    RESPECTED SIR/MADAM,

                                                         I  KIRAN  STUDYING MTECH AND I PRESENTLY DOING PROJECT ON BLDC MOTOR AND THE PROBLEM IS WHEN THE CODE FOR SEED-DEC2812(DSP TMS320LF2812). THE HEADER FILES  FOR SEED-DEC2812(DSP TMS320LF2812)  ARE NOT WORKING PROPERLY MEANS  SOME REGISTERS ARE NOT WORKING AND CANNOT CORRECTLY MAPPED

    LIKE THIS

    IMR        .set        0004h
    IFR        .set        0006h
    SCSR1        .set        7018h
    SCSR2        .set        7019h

            SO,PLEASE PROVIDE HEADER FILES FOR SEED -DEC2812(DSP TMS320LF2812)

     

    I am not familiar with the particular board you mention or the code that comes with the board.  I did a google search which pointed me to this page - they may be able to help with any specific software that came with the board: http://www.seeddsp.com/

    TI Supplies C headerfiles that can also be included in assembly files.  For the download and more information, please refer to the following Wiki:

    http://processors.wiki.ti.com/index.php/Getting_Started_with_C2000_Links#Software:_Peripheral_Examples.2C_Libraries_and_Application_Notes

    Regards,

    Lori