Part Number: TMS320F28379S
Tool/software: Code Composer Studio
Hi,
I got an error when debug the board using MCU TMS320F28379S.
C28xx_CPU1: Error: (Error -1044 @ 0x0)
The error happened in running program after successful loading.
My program can only run in 20MHz. If my PLL frequency exceed 50MHz, the program can't run and console report the error code.
I have tried to check the integrity of JTAG pins, but it didn't work.