Part Number: TMS320F28034
Would like to use the CAN timeout feature and monitor at 250 kbps the reception of a CAN message
ECanaMOTORegs.MOTO16 is 2500 means 10 ms
ECanaMOTSRegs.MOTS16 is 5000 means 20 ms
ECanaShadow_s.CANTOC.bit.TOC16 is set
but ECanaRegs.CANTOS.bit.TOS16 is reset steadily
Was is going wrong here?
What is the function of ECanaShadow_s.CANTRS.bit.TRS16 in context of a reception?
Do we have example code for that?
Regards, Bernd