This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CTS / RTS Hardware Flow Control

I have an application that requires CTS/RTS flow control in order to send bulk data at relatively high UART speeds.  Since the C2000 does not have flow control built into the peripheral, I have implemented it by checking the status of an input line before sending a byte.  Since the device also seems to buffer a few bytes with or without the FIFO turned on, I have also used logic to make sure that the FIFO buffer is empty.  It still seems that very occasionally, I am overrunning the receive buffer by about 2 bytes out of every few million.  I have posted the code I am using below in case anybody sees any errors.

As I am writing this, I am also considering the possibility of disabling the SCI peripheral clock whenever the flow control from the module is asserted.  I do not want to lose any buffered bytes, however.  Is this a good or bad idea?  Any other suggestions?

Here is my current code:

void Scib_xmit(int a)

{ 

while(GpioDataRegs.GPADAT.bit.GPIO10 == 1 || ScibRegs.SCICTL2.bit.TXRDY == 0 || ScibRegs.SCIFFTX.bit.TXFFST != 0)

{

}

  ScibRegs.SCITXBUF = a;

}