Part Number: TMS320F28335
Other Parts Discussed in Thread: C2000WARE
Hi,
I think I have answered my own question here, but being fairly new to the TI platform want to be certain, especially as the amount of code I will have to write would seem to depend on the answer.
I just finished a project which used the F280049M dsp.
This project used the F28004x Support Library provided by my installed C200Ware software package and utilized the many handy high level peripheral functions that are available in the driverlib.
I am now working on a project which uses the F28335 dsp.
Reading the C200Ware documentation shows that it supports the F2833x dsp and there is indeed that part listed in the device_support folder.
However the F28004x Support Library (driverlib.lib), which I used for the F280049M dsp would appear to not be available for the F28335 dsp. Is that correct?
Instead I have only the much more limited functionality provided by the F2833x Support Library source files (ie DSP2833x_EPwm.c), etc.
So a handy function like EPWM_setActionQualifierAction(), available in the F28004x Support Library, does not exist for the F2833x dsp. I would have to write the code that would have been handled by a function like this.
Is my understanding correct?
Any idea why there is no comparable higher level library interface available for the F28335 dsp?
Thank you!
Mark