Hi everyone,
I need to convert 10 signals at same time and after that to process into the DSP,
I have two options:
1) Using 10 sample and hold, all the sample hold will sampling their signals at the same time, after the Sample Hold finish the DSP will convert
each sample one after one, my question is, wich Sample Hold to use?
2) Using 10 ADC converters with 1 channel. after all ADC finish the convertion the DSP will get the data, by one bus I2C or SPI. My second question wich ADC module to use?
P.S. I need to get all signals at same time at 1khz rate.
Thanks!