This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8312-C2-KIT: Issues with DRV8312-C2-KIT and Simulink examples

Part Number: DRV8312-C2-KIT

Hi I've downloaded an example of FOC from this link https://www.mathworks.com/help/supportpkg/texasinstrumentsc2000/examples/permanent-magnet-synchronous-motor-field-oriented-control.html. I can get it to upload to the board correctly but it does not run correctly. At first the motor just vibrates and I have to turn the switches to reset and let it sit for a minute then it gives me a signal that spins the motor but the motor vibrates quite a bit and the signal doesn't look like a normal FOC signal. Anyone have any experience or advice? I don't know if this is relevant but I have gotten all of the instaspin labs to work for my current set up so I don't think the problem is with the hardware.