Part Number: TMS320F28379D
Other Parts Discussed in Thread: TLK110
Tool/software: Code Composer Studio
Hi,
Now I have designed TMS320F28379D hardware which is used to develop EtherCAT protocol.
PHY is TLK110,esc is ET1100, EEPROM is 24LC16.
Now I download the first 10 words info. into EEprom, and ET1100 can read register like 0x0140 , 0x502 and so on.
Next step , my hardware as EtherCAT slave will be connected to beckhoff IPC.
But I am not sure if PHY register is needed to read and write when the net wire is connected to slave?
I refer TMDSECATCNCD379D example code ,and do not find any code about PHY setup . So I need help how to do next?
Make better if you can supply some reference or datasheet to develop. Thanks in advance.
Best Regards!
Richie