This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28035: TMS320F28035

Part Number: TMS320F28035
Other Parts Discussed in Thread: C2000WARE

Tool/software: Code Composer Studio

I unable to debug below code

#include "DSP2803x_Device.h"
#include "DSP2803x_Examples.h"

//---------------------------------------------------------------------------
// InitLin:
//---------------------------------------------------------------------------
// This function initializes the LIN to a known state.
//

void InitLin(void)
{
InitLina();
}

void InitLina(void)
{
EALLOW;

//Initialize LIN

//Reset module and release reset.
LinaRegs.SCIGCR0.bit.RESET = 0;
LinaRegs.SCIGCR0.bit.RESET = 1;

//LIN into software reset mode
LinaRegs.SCIGCR1.bit.SWnRST = 0;

//Select LIN Mode
LinaRegs.SCIGCR1.bit.LINMODE = 0;

//Configure LIN mode

LinaRegs.SCIGCR1.bit.CLK_MASTER = 1; // 1-->Master, 0-->Slave
LinaRegs.SCIGCR1.bit.ADAPT = 0; // Fixed baud rate
LinaRegs.SCIGCR1.bit.COMMMODE= 0; // ID bits 4 and 5 not used for length control
LinaRegs.SCIGCR1.bit.CONT = 1; // Continue on Emulation suspend
LinaRegs.SCIGCR1.bit.CTYPE = 1; // LIN 2.0 Enhanced checksum used
LinaRegs.SCIGCR1.bit.HGENCTRL = 1; // ID match vs LinaRegs.bit.IDSLAVETASKBYTE
LinaRegs.SCIGCR1.bit.LOOPBACK = 0; // External communication mode
LinaRegs.SCIGCR1.bit.MBUFMODE = 1; // Buffered mode
LinaRegs.SCIGCR1.bit.PARITYENA = 1; // Check received ID for parity
LinaRegs.SCIGCR1.bit.RXENA = 1; // Enable RX pin
LinaRegs.SCIGCR1.bit.TXENA = 1; // Enable TX pin

//More LIN configs
LinaRegs.SCIGCR2.bit.CC = 1; // Validate checksum

//Set all interrupts to disabled
LinaRegs.SCICLEARINT.all = 0xFFFFFFFF;

//Baud Rate Settings - 60MHz device

LinaRegs.BRSR.bit.SCI_LIN_PSL = 96; // 19.2 kbps
LinaRegs.BRSR.bit.M = 11;
LinaRegs.MBRSR = 92; //20kHz (max autobaud rate)

//LIN Character Size and Length
LinaRegs.SCIFORMAT.bit.LENGTH = 0; // 8 bit transmission/response

//SYNC Field Configuration
LinaRegs.LINCOMP.bit.SBREAK = 5; // Sync break is 13 + 5 = 18 Tbits
LinaRegs.LINCOMP.bit.SDEL = 3; // Sync delimiter is 1 + 3 = 4 Tbits

//LIN MASK Configuartion
LinaRegs.LINMASK.bit.TXIDMASK = 0xFF; // Mask ID so TX match will always happen
LinaRegs.LINMASK.bit.RXIDMASK = 0xFF; // Mask ID so RX match will always happen

//IODFT Configuarations
LinaRegs.IODFTCTRL.bit.IODFTENA = 0x0; // IODFT testing module disabled
LinaRegs.IODFTCTRL.bit.LPBENA = 0; // IODFT loopback disabled

//Release SCI from software reset state - End of Config
LinaRegs.SCIGCR1.bit.SWnRST = 1;

EDIS;
}


//---------------------------------------------------------------------------
// GenIdParity:
//---------------------------------------------------------------------------
// This function generates the ID parity bits and appends them to the ID.
// Call this function on a desired ID before header generation in master
// mode when LinaRegs.SCIGCR1.bit.PARITYENA is set.
//
Uint16 P0;
Uint16 P1;

Uint16 GenIdParity(Uint16 id)
{
P0 = ((id << 6) ^ (id << 5) ^ (id << 4) ^ (id << 2)) & BIT6;
P1 = (((id << 6) ^ (id << 4) ^ (id << 3) ^ (id << 2)) & BIT7) ^ BIT7;
return id | P0 | P1;
}

//---------------------------------------------------------------------------
// Example: InitLinGpio:
//---------------------------------------------------------------------------
// This function initializes GPIO pins to function as LIN pins
//
// Each GPIO pin can be configured as a GPIO pin or up to 3 different
// peripheral functional pins. By default all pins come up as GPIO
// inputs after reset.
//
// Caution:
// Only one GPIO pin should be enabled for LIN TX operation.
// Only one GPIO pin shoudl be enabled for LIN RX operation.
// Comment out other unwanted lines.

void InitLinGpio()
{
InitLinaGpio();
}

void InitLinaGpio()
{
EALLOW;

/* Enable internal pull-up for the selected pins */
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.

GpioCtrlRegs.GPAPUD.bit.GPIO9 = 0; // Enable pull-up for GPIO9 (LIN TX)
// GpioCtrlRegs.GPAPUD.bit.GPIO14 = 0; // Enable pull-up for GPIO14 (LIN TX)
// GpioCtrlRegs.GPAPUD.bit.GPIO18 = 0; // Enable pull-up for GPIO18 (LIN TX)
// GpioCtrlRegs.GPAPUD.bit.GPIO22 = 0; // Enable pull-up for GPIO22 (LIN TX)

GpioCtrlRegs.GPAPUD.bit.GPIO11 = 0; // Enable pull-up for GPIO11 (LIN RX)
// GpioCtrlRegs.GPAPUD.bit.GPIO15 = 0; // Enable pull-up for GPIO15 (LIN RX)
// GpioCtrlRegs.GPAPUD.bit.GPIO19 = 0; // Enable pull-up for GPIO19 (LIN RX)
// GpioCtrlRegs.GPAPUD.bit.GPIO23 = 0; // Enable pull-up for GPIO23 (LIN RX)

/* Set qualification for selected pins to asynch only */
// Inputs are synchronized to SYSCLKOUT by default.
// This will select asynch (no qualification) for the selected pins.

GpioCtrlRegs.GPAQSEL1.bit.GPIO11 = 3; // Asynch input GPIO11 (LINRXA)
// GpioCtrlRegs.GPAQSEL1.bit.GPIO15 = 3; // Asynch input GPIO15 (LINRXA)
// GpioCtrlRegs.GPAQSEL2.bit.GPIO19 = 3; // Asynch input GPIO19 (LINRXA)
// GpioCtrlRegs.GPAQSEL2.bit.GPIO23 = 3; // Asynch input GPIO23 (LINRXA)


/* Configure LIN-A pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be LIN pins.
// Only one set of pins should be enabled at any time for LIN operation.

GpioCtrlRegs.GPAMUX1.bit.GPIO9 = 2; // Configure GPIO9 for LIN TX operation (2-Enable,0-Disable)
// GpioCtrlRegs.GPAMUX1.bit.GPIO14 = 2; // Configure GPIO14 for LIN TX operation (2-Enable,0-Disable)
// GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 2; // Configure GPIO18 for LIN TX operation (2-Enable,0-Disable)
// GpioCtrlRegs.GPAMUX2.bit.GPIO22 = 3; // Configure GPIO19 for LIN TX operation (3-Enable,0-Disable)

GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 2; // Configure GPIO11 for LIN RX operation (2-Enable,0-Disable)
// GpioCtrlRegs.GPAMUX1.bit.GPIO15 = 2; // Configure GPIO15 for LIN RX operation (2-Enable,0-Disable)
// GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 2; // Configure GPIO19 for LIN RX operation (2-Enable,0-Disable)
// GpioCtrlRegs.GPAMUX2.bit.GPIO23 = 3; // Configure GPIO23 for LIN RX operation (3-Enable,0-Disable)

EDIS;
}

//===========================================================================
// End of file.
//===========================================================================