This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Respected sir,
I am working on TMS320F28069M launchpad. I am trying to run the LED blinking code for this device.
But while setting the target target configuration file I found that TMS320F28069M controller is not present in the list so I have selected TMS320F28069.
While debugging I am facing the problem as below
(Error -1135 @ 0x0)
The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation.
(Emulation package 8.0.27.9) "
The development is in the CCS v8 and the debug probe is XDS100v2.
I tried to run the code by taking another probe for debugging but facing the same problem.
I have also tried the LED blinking for this launchpad using Energia software. While selecting the target board I get to know that
TMS320F28069M launchpad is not present in Energia also so I have selected TMS320F28069 launchpad and faced the same problem
" error: C28xx: Error connecting to the target: (Error -1135 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 6.0.14.5) "
kindly request you to help me out.
Regards,
Nisha
Nisha,
Please continue to use the F28069 as the target for the LAUNCHXL-F28069M, in terms of emulation the devices are identical.
Please take a look at the following app note http://www.ti.com/lit/an/spracf0/spracf0.pdf , I've tried to capture many common JTAG connectivity issues; following the steps will either resolve the issue or get us to a known place in terms of debug so I can be most helpful in future correspondence.
Best,
Matthew