Part Number: TMDSCNCDH52C1
Other Parts Discussed in Thread: UNIFLASH, CONTROLSUITE
Hello,
I'm new to F28M35x series devices and I had been programming above Concerto control card hundred of times without any issue. Few weeks ago, loading program error occurred when programming C28x processor in flash mode. After that same error occurred and I used a new control card after that. Today the second one also gave the same error and not able to program C28x after that in any way.
Following are noted,
1. Arm-M3 processor work fine, without any issue and can be programmed
2. Attempted erasing flash of C28x using both CCS & UniFlash, both were unsuccessful
3. Always give the error code 1156 @ 0x8050, Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device.
It would be very helpful if you can provide a solution to this since total project is at stuck due to this
Thanks,
Tharindu