This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28069M: SCI Connection of MCU to Simulink: Always timeouts?

Part Number: LAUNCHXL-F28069M


I'm attempting to write a python script to communicate directly with the board but I am running into timeout issues. I've already got a script set up to send and receive serial signals on the correct COM channel and those work for cases where I am only sending one signal or only receiving one signal. Currently I have an simulink model (see attached photo) that receives a signal multiplies it by 2 and sends it back again. When I run my script it is sending out the correct input but not getting the correct output after the first cycle. After the initial values are multiplied by 2 the SCI receive block timeouts and starts just sending a default value. Is there anyway around this issue?