Part Number: TMS320F28379D
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Hello everyone,
I'm having some problems while running the example timed_led_blink_cpu01 from controlsuite.
I've made some modifications to the original project, like adding to my code an .cmd file (2837x_RAM_lnk_cpu1.cmd) and modified the length of RAMGS4 from 0x001000 to 0x12000, and renamed it to LOG.
After that I've commented the other RAMGS lines until the RAMGS15.
I'm also adding in the LEDBLINK.c code, inside the cpu_timer0_isr void the function logger(), and including the logger files .h and .asm to the project.
When I build the project It doesn't show any error, but it does not work since apparently the code is stuck on the F2837xD_SysCtrl.c code in the 556 line: while(ClkCfgRegs.SYSPLLSTS.bit.LOCKS != 1)
Does anyone knows how to fix and/or why this problem is occuring ?
Thanks in advance,
Izabela.