Part Number: F28M36P63C2
Tool/software: Code Composer Studio
Hello,
I have a query about something i read on the Technical reference manual regarding the C28 SPI interface with regards to setting the SPI Baudrate. I am trying to SPI write to an LCD , with a transfer every 500 ms.
I am trying to decide the appropriate SPI BRR value. and i am following the below steps
#define CPU_FREQ 150E6 // 150MHz #define SPI_BAUDRATE 2 // 2 Hz #define LSPCLK_FREQ (CPU_FREQ/4) #define SPI_BRR (LSPCLK_FREQ/SPI_BAUDRATE)-1
Is this accurate?
Thank you,
Srini