Part Number: TMS320F28069
Other Parts Discussed in Thread: TMDSDOCK28069, CONTROLSUITE, C2000WARE, LAUNCHXL-F28069M
The i2c sample program given in the control suit is not working. what could be the issue? i am using 28069 control stick with usb dociing station of rev 2.0 wherein jp9 has to be connected between processor line and the FTD chip .Even after this it is not working
Do I have to connect the jumper ?
I am not able to do single stepping if i try to do ? is there any standard working program available. ? pl do send it at the earliest.
And also pl clarify how to see the result? using memview only ????
Thanking you,
Regards
Sundari