Hi,
We have an old product line where we are considering changing from a F2812 to F28335 to get floating point. Some of the code is very old and it was developed with tools no longer available.
1) We were wondering if we can run the old F2812 object code on the 28335 and have it run
2) If not, can we just run the original source code through the new compiler for the 28335? My guess is that the header files would have to change, but are the chip internals similar enough that recompiled code would run?
Thanks for any input,
Lloyd