Part Number: TMS320F28377S
Other Parts Discussed in Thread: OPA320, OPA350
Tool/software: Code Composer Studio
Hi everyone!
I am using TI's micom, TMS320F377S to read analog voltage using internal ADC with following environment
- 12 bit resolution
- 200 MHz internal clock
At low voltage range (eg. from 0.4 to 0.6), converted voltage integers are accurate
The measured accuracy is near to 1 LSB ( = 3.3V/4096 = 0.8 mV).
But, at high voltage range (eg. from 3 to 3.2), converted voltage integers are not not accurate.
The measured accuracy is near to 25 LSB ( = 20 mV).
Would you let me know to achieve high accuracy in high voltage range?
Thanks. Best Regards