Part Number: TMS320F28032
Hello,
I've read through the data sheet and there wasn't really a clean cut formula to determine the high-resolution PWM bits in order to determine the resolution. Is there any one that knows of a formula for it?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28032
Hello,
I've read through the data sheet and there wasn't really a clean cut formula to determine the high-resolution PWM bits in order to determine the resolution. Is there any one that knows of a formula for it?
Thanks!
user4997907,
There is no formula for the step size of the HRPWM. In our documentation we refer to this as a MEP step size. The datasheet has a typical and a max value published in section 6.9.10.1 "HRPWM Electrical Data/Timing".
Note 1:The MEP step size will be largest at high temperature and minimum voltage on VDD. MEP step size will increase with higher temperature and lower voltage and decrease with lower temperature and higher voltage.
Note 2:Each MEP step is not exactly the same size some will be larger than others.
Regards,
Cody
Hi,
do you mean how to determine bit count from non power of two maximum count N? It's log(N) / log(2). Full steps at 60MHz clock and 300kHz PWM is 200? 180ps microsteps in 1/60MHz - about 92. So N = 200 * 92, resolution bits ~14.1. In symmetric mode since up and down count is the same, resolution is 2 times lower, resolution bits is one less, ~13.1 bits.
Edward
user4997907 said:How are the resolution bits calculated in the documentation for HRPWM then?
When the F2803x device was first produced it underwent validation. During this validation high-accuracy equipment was used to observe the PWM's output as the HRPWM was configured and used across a large number of operating conditions. Several engineers then carefully reviewed the data taken and placed those numbers into the datasheet.
user4997907 said:Let's assume we have a fixed MEP SIZE of 180ps, Operating at 60Mhz with a desired PWM frequency of 300kHz, using the UP DOWN Symmetrical Scheme?
Sorry, I do not understand what this question is asking. Operating at 60 Mhz will not affect your PWM's resolution. You can use the HRPWM to generate a PWM at a frequency of 300 kHz signal. Up-Down count mode should be OK.
Regards,
Cody
Christian,
user4997907 said:The MEP changes during run time, which is why the SFO function is required. Is that no so?
The MEP does change during runtime, and yes the SFO will help compensate for it. It however does not allow you to adjust it to 10 MEP steps per SYSCLK period.
user4997907 said:I'm confused how the Master Clock doesn't affect resolution?
When talking about the ePWM; you are correct, exactly as you have pointed out, SYSCLK(Master Clock) does affect the resolution. When talking about HRPWM; the period of SYSCLK does not change the length of a MEP step size, the two are completely unrelated.
Regards,
Cody