Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE
Tool/software: TI C/C++ Compiler
Dear support gurus!
I am developing a project that exploits uPP interface for bidirectional communication of TMS230F u-controller and FPGA. I try to test uPP in transmission mode with standalone board LAUNCHXL_F28377S before using FPGA, but I have discovered the following problem: the transmission state does not recover after WAIT signal changes back to high level.
The brief description of test project is given below:
The test project is modified on base of example «upp_sdr_tx» from C2000Ware_1_00_01_00 for LAUNCHXL_F28377S. In project properties Predefined Symbols are defined as _LAUNCHXL_F28377S. The transmitter is not connected to the FPGA board. The following changes are made in project:
- parameters LINE_CNT, WORD_CNT, BYTE_CNT, WIN_CNT are changed;
- Wait signal is enabled;
- Wait signal is set as Active low;
- Transmitted value is set as 0x1;
- Periodical data transfer is programed by for(;;); cycle.
Initially the test project operates correctly as I can observe the expected signals CLOCK, DATA, WAIT and ENABLE by means of oscilloscope. The WAIT signal is not connected to receiver and I can detect 3 V potential. When I short circuits WAIT pin to the ground I can see that transmission stops, but when circuit opens the transmission does not begins automatically. Transmission starts only after RESET and RESTART commands.
Could you please help me fix the attached program to restore transmission after setting WAIT signal back to high value.
//#############################################################################
//
// FILE: upp_sdr_tx_cpu01.c
//
// TITLE: upp transmit example for F2837xS
//
//! \addtogroup cpu01_example_list
//! <h1> UPP Single Data Rate Transmit (upp_sdr_tx) </h1>
//!
//! This example sets up the F2837xS board's UPP with the single-data-rate(SDR)
//! interface as a transmitter.
//!
//! \b Important: In order to run this example, two F2837xS boards are required.
//! All the UPP pins from one board to the other must be connected with common
//! ground. One board must be loaded with this example code and the other board
//! must be loaded with the "upp_sdr_rx" example.
//!
//! \b Instructions:
//! # Load the "upp_sdr_tx" on board 1
//! # Load the "upp_sdr_rx" on board 2
//! # Run the "upp_sdr_rx" code on board 2 (Needs to be run before the tx code)
//! # Run the "upp_sdr_tx" code on board 1
//!
//! \b Watch \b Variables: \n
//! - \b TEST_STATUS - Equivalent to \b TEST_PASS if test finished correctly,
//! else the value is set to \b TEST_FAIL
//! - \b ErrCount - Error counter
//!
//
//
// |-----------| |-----------|
// | |=====D0-D7=====| |
// | Device |-----CLK-------| Device |
// | Board-1 | | Board-2 |
// | TX |-----ENABLE----| RX |
// | |-----START-----| |
// |-----------| |-----------|
//
//#############################################################################
// $TI Release: F2837xS Support Library v3.01.00.00 $
// $Release Date: Mon May 22 15:44:59 CDT 2017 $
// $Copyright:
// Copyright (C) 2014-2017 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################
// Included Files
//
#include "F28x_Project.h"
#include "F2837xS_Upp_defines.h"
// Defines
//
#define TEST_PASS 0xABCDABCD
#define TEST_FAIL 0xDEADDEAD
#define LINE_CNT 1//4//
#define WORD_CNT 6
#define BYTE_CNT WORD_CNT*2//64//
#define WIN_CNT 1//8//
#define WIN_BYTE_CNT WORD_CNT*2*LINE_CNT//256//
#define WIN_WORD_CNT WORD_CNT*LINE_CNT//128//
#define LINEOFFSET 0
#define TAKE_NNN 0x1//0xAAAB // ������� �������� ���� �� TMS � FPGA
#define BUTTON 59 // GPIO59 J2 Pin14
// Globals
//
volatile long int ErrCount;
volatile long int TEST_STATUS = TEST_FAIL;
volatile long int eow_int_cnt = 0;
volatile long int eol_int_cnt = 0;
volatile long int RdValue = 0;
volatile long int WrValue = 0;
volatile int InitTxMsgRam = 0;
// Function Prototypes
//
extern void InitUpp1Gpio(void);
extern void SoftResetUpp(void);
interrupt void local_UPPA_ISR(void);
int i,iii=0,jj=0,kk=0,ll=0,mm=0,nn=0,p=0,r=0,s=0,btn=0,mem=0,data=1,tmp=0;
// Main
//
void main(void)
{
TEST_STATUS = TEST_FAIL;
ErrCount = 0x0;
GPIO_SetupPinMux(BUTTON, GPIO_MUX_CPU1, 0);//
GPIO_SetupPinOptions(BUTTON, GPIO_INPUT, GPIO_PUSHPULL | GPIO_INVERT | GPIO_ASYNC);//, |GPIO_PULLUP
// Initialize System Control
InitSysCtrl();
DINT;
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flaLS
// are cleared.
// This function is found in the F2837xS_PieCtrl.c file.
//
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
EALLOW;
IER = 0x0000;
IFR = 0x0000;
EDIS;
// Initialize the PIE vector table with pointers to the shell Interrupt
// LService Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2837xS_DefaultIsr.c.
// This function is found in F2837xS_PieVect.c.
InitPieVectTable();
EALLOW;
PieVectTable.UPPA_INT = &local_UPPA_ISR;
// Enable the Interrupt No 8.
IER = M_INT8 ;
// Enable Interrupt for UPPA Interrupt.
PieCtrlRegs.PIEIER8.bit.INTx15=1;
// Enable PIE & CPU level Interrupts.
EnableInterrupts();
// Issue Soft Reset (internal) to uPP.
SoftResetUpp();
// Configure the GPIO muxing for uPP pins.
// mux = 15, �.�. GPAGMUX1 = 3 � GPAMUX1 = 2. disable pull-up (GPAPUD = 1),
// Async input (no Sync or Qualification) GPAQSEL1 = 3
InitUpp1Gpio();
// Initialize the TX MSG RAM. #define uPP_TX_MSGRAM_SIZE 512 ��� ���������� ������ 512�16
for (i = 0; i < uPP_TX_MSGRAM_SIZE ; i+=1)
*(Uint32 *)(uPP_TX_MSGRAM_ADDR + i) = 0;
*(Uint32 *)(uPP_TX_MSGRAM_ADDR) = data;//TAKE_NNN;
// Configure uPP for TX
UppRegs.IFCFG.bit.CLKDIVA = 0xF;//0x4; // 0x4: Div8. Clock divider for transmit mode: TX_IOCLK = CHIP_CLK / 2(N+1)
UppRegs.IFCFG.bit.CLKINVA = 1; // 1: Clock is inverted
UppRegs.CHCTL.bit.MODE = uPP_TX_MODE; // Setup for TX. 01: Pure output transmit mode.
UppRegs.CHCTL.bit.DRA = uPP_SDR; // SDR mode 0: Single Data Rate (SDR)
UppRegs.IFIVAL.all = 0x0000; //Idle Value. When in transmit mode, this field holds the value that will
// be driven out when the channel is idle
GpioCtrlRegs.GPAPUD.bit.GPIO10 = 0; // 1: Disable pull-up on GPIO10 (uPP_WAIT)
UppRegs.IFCFG.bit.WAITA = 1; // 1: Enable (Tx: honor wait)
UppRegs.IFCFG.bit.WAITPOLA = 1; // 1: Active Low. 0: Active High.
for(;;)
{
*(Uint32 *)(uPP_TX_MSGRAM_ADDR) = data;//TAKE_NNN;
// Enable EOL/EOW interrupt
UppRegs.INTENSET.bit.EOLI = 1; // 1: Interrupt enable for end-of-line condition.
UppRegs.INTENSET.bit.EOWI = 1; // 1: Interrupt enable for end-of-line condition.
UppRegs.GINTEN.bit.GINTEN = 1; // 1= uPP generates interrupt to if interrupt flag gets set
UppRegs.PERCTL.bit.PEREN = 1; //1: Enable/Resume the uPP module
// Setup DMA channel
UppRegs.CHIDESC0 = uPP_TX_MSGRAM_ADDR;// Starting address of the DMA Channel I transfer.
UppRegs.CHIDESC1.bit.LCNT = LINE_CNT; // Number of lines in a window for DMA Channel I transfer
UppRegs.CHIDESC1.bit.BCNT = BYTE_CNT; // Number of bytes in a line for DMA Channel I transfer
UppRegs.CHIDESC2.all = LINEOFFSET;//BYTE_CNT;// // Line Offset Address. Offset from the current line starting address to the next line
// starting address for DMA Channel I transfers
PieCtrlRegs.PIEACK.all = PIEACK_GROUP8;// = 0�80
while (eow_int_cnt < WIN_CNT); // WIN_CNT = 8 // eow_int_cnt ������������ � ����������� ����������
// Disable the uPP to stop transmission after expected window count is done.
UppRegs.PERCTL.bit.PEREN = 0; // 0: Disable/Suspend the uPP module
// asm(" ESTOP0");
eow_int_cnt = 0;
eol_int_cnt = 0;
// Determine example test status
if (ErrCount == 0x0)
TEST_STATUS = TEST_PASS;
}
}
// local_UPPA_ISR - UPPA Interrupt Service Routine (ISR)
interrupt void local_UPPA_ISR(void)
{
// To receive more interrupts from this PIE group, acknowledge this interrupt
int i;
// jj++;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP8;// = 0�80
if (UppRegs.GINTFLG.all != 0x0) // 1: Interrupt has been generated.
{
// kk++;
if(UppRegs.ENINTST.bit.EOWI == 0x1) //Check for EOW Interrupt flag
{ // 1: End Of Window event happened
// ll++;
eow_int_cnt++;
if (eow_int_cnt < (WIN_CNT - 1)) // WIN_CNT = 8
{
InitTxMsgRam = 1;
}
//Enable EOL interrupt ��������� ���� ���������� �� Window, ������ ���� � ���������� EOL
UppRegs.INTENSET.bit.EOLI = 1; // Interrupt enable for end-of-line condition
//Clear the Status for EOW Interrupt Writing 1 will clear the interrupt status
UppRegs.ENINTST.all = uPP_INT_EOWI; // =8; Interrupt enable status for end-of-Window condition.
if (UppRegs.ENINTST.bit.EOWI != 0) // ���� �� ��������� ����?
{
ErrCount++;
asm (" ESTOP0");
for(;;);//�������� �����, ���� ������
}
}
if(UppRegs.ENINTST.bit.EOLI == 0x1) // Check for EOL Interrupt Flag
{// ����� EOWI �� ����, � EOLI ���������
// nn++;
eol_int_cnt++;
// Disable EOL Interrupt. Writing 1 will clear the interrupt status
UppRegs.ENINTST.all = uPP_INT_EOLI;// = 0x10; Interrupt enable status for end-of-line condition.
if (UppRegs.ENINTST.bit.EOLI != 0)// ���� ���� �� ���������
{
ErrCount++;
asm (" ESTOP0");
for(;;);//�������� �����, ���� ������
}
UppRegs.INTENCLR.all = uPP_INT_EOLI;// Interrupt clear for end-of-line condition.
// Writing 1 will disable the interrupt
if (UppRegs.INTENSET.bit.EOLI != 0)
{
ErrCount++;
asm (" ESTOP0");
for(;;);//�������� �����, ���� ������
}
// Initialize the Channel Descriptor for Next window transfer.
if (eow_int_cnt < (WIN_CNT -1))//���� �� ��� ���������
{
// mm++;
if (eow_int_cnt%2)//������� �� �������
{
if(InitTxMsgRam == 1)
{
for (i = 0; i < WIN_WORD_CNT ; i+=2)
{
WrValue = WrValue + 0x12345678;
*(Uint32 *)(uPP_TX_MSGRAM_ADDR + i) = WrValue;
}
InitTxMsgRam = 0;
}
UppRegs.CHIDESC0 = uPP_TX_MSGRAM_ADDR;//����� � �������� ������ ������������. ���������� �����������������
UppRegs.CHIDESC1.bit.LCNT = LINE_CNT;
UppRegs.CHIDESC1.bit.BCNT = BYTE_CNT;
UppRegs.CHIDESC2.all = LINEOFFSET;//BYTE_CNT;//
}
else
{
if(InitTxMsgRam == 1)
{
for (i = 0; i < WIN_WORD_CNT ; i+=2)
{
WrValue = WrValue + 0x12345678;
*(Uint32 *)((uPP_TX_MSGRAM_ADDR +
WIN_WORD_CNT) + i) = WrValue;
}
InitTxMsgRam = 0;
}
UppRegs.CHIDESC0 = uPP_TX_MSGRAM_ADDR + (LINE_CNT *
BYTE_CNT);
UppRegs.CHIDESC1.bit.LCNT = LINE_CNT;
UppRegs.CHIDESC1.bit.BCNT = BYTE_CNT;
UppRegs.CHIDESC2.all = LINEOFFSET;//BYTE_CNT;//
}
}
}
// Clear Global Interrupt.
RdValue = UppRegs.ENINTST.all;
UppRegs.GINTCLR.bit.GINTCLR = 1;
if (UppRegs.GINTFLG.all != 0x0)
{
ErrCount++;
asm (" ESTOP0");
for(;;);//�������� �����, ���� ������
}
}
}
//
// End of file
//
With respect,
Alexander M