Part Number: INSTASPINUNIVERSALGUI
Hi
I have a custom BLDC motor Im running on the Instaspin HV board. When running though the identify routine, it runs loud and choppy, Ive played around with Estimation Freq = 100 and Motor Max Freq = 330 and it does make a differance, just not smooth.
Also its not consistant when Identifying the motor, it misses some of the tests.
The specs on the motor listed below
3 Phase
110VAC
SIN BEMF 30V/kRPM
Torque constant 0.2866 Nm/A
5000 RPM
My goal is to test the motor running back and forth maxium torque, when it hits a limit switch it reverses direction. Do you no of any labs that do a test close to that.