Part Number: TMS320F28379D
Hi,
I've noticed that the TRM fro F28379D does refer to ADCIN13 when talking about Internal Temperature sensors, but there is no pin ADCIN13, only ADCIN14 and ADCIN15.
Can anyone describe how I can relate ADCB0 to a specific channel ADCIN0-15?
I am very confused about them.
Also, I've noticed that the current version of TI's PinMux tool is showing incorrect pin usage. For example, if you create a new configuration for TMS240F28379D, 176 pin PTP package, pin 33 is shown as ADCINC0. However, if you look at the Datasheet for F2837D, the ADCINC0 is never mentioned. The pin 33 is shown as VREFLOA.