Tool/software: TI C/C++ Compiler
Hi,
I want to interface 25lc256 eeprom with TMS320F28075. I am using I2C_b peripheral with GPIO40 and 41 Pins . I have done changes accordingly but not able to communicate with slave.Please check attach file .
Regards,
Sagar
//###########################################################################
//
// FILE: Example_2807xI2C_eeprom.c
//
// TITLE: I2C EEPROM Example
//
//! \addtogroup cpu01_example_list
//! <h1>I2C EEPROM Example (i2c_eeprom)</h1>
//!
//! This program will write 1-14 words to EEPROM and read them back.
//! The data written and the EEPROM address written to are contained
//! in the message structure, I2cMsgOut1. The data read back will be
//! contained in the message structure I2cMsgIn1.
//!
//! \b External \b Connections \n
//! - This program requires an external I2C EEPROM connected to
//! the I2C bus at address 0x50.
//!
//
//###########################################################################
// $TI Release: F2807x Support Library v200 $
// $Release Date: Tue Jun 21 14:11:45 CDT 2016 $
// $Copyright: Copyright (C) 2014-2016 Texas Instruments Incorporated -
// http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################
//
// Included Files
//
#include "F28x_Project.h"
//
// Defines
//
#define I2C_SLAVE_ADDR (0x50)
#define I2C_NUMBYTES (2)
#define I2C_EEPROM_HIGH_ADDR (0x00)
#define I2C_EEPROM_LOW_ADDR (0x30)
//
// Globals
//
struct I2CMSG I2cMsgOut1={ I2C_MSGSTAT_SEND_WITHSTOP,
I2C_SLAVE_ADDR,
I2C_NUMBYTES,
I2C_EEPROM_HIGH_ADDR,
I2C_EEPROM_LOW_ADDR,
0x12, // Msg Byte 1
0x34}; // Msg Byte 2
struct I2CMSG I2cMsgIn1={ I2C_MSGSTAT_SEND_NOSTOP,
I2C_SLAVE_ADDR,
I2C_NUMBYTES,
I2C_EEPROM_HIGH_ADDR,
I2C_EEPROM_LOW_ADDR};
struct I2CMSG *CurrentMsgPtr;
Uint16 PassCount;
Uint16 FailCount;
//
// Function Prototypes
//
void I2CA_Init(void);
Uint16 I2CA_WriteData(struct I2CMSG *msg);
Uint16 I2CA_ReadData(struct I2CMSG *msg);
__interrupt void i2c_int1a_isr(void);
void pass(void);
void fail(void);
//
// Main
//
void main(void)
{
Uint16 Error;
Uint16 i;
CurrentMsgPtr = &I2cMsgOut1;
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2807x_SysCtrl.c file.
//
InitSysCtrl();
//
// Step 2. Initialize GPIO:
// This example function is found in the F2807x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
InitGpio();
//
// For this example, only init the pins for the SCI-A port.
// These functions are found in the F2807x_Gpio.c file.
//
GPIO_SetupPinMux(32, GPIO_MUX_CPU1, 1);
GPIO_SetupPinMux(33, GPIO_MUX_CPU1, 1);
//
// Step 3. Clear all __interrupts and initialize PIE vector table:
// Disable CPU __interrupts
//
DINT;
//
// Initialize PIE control registers to their default state.
// The default state is all PIE __interrupts disabled and flags
// are cleared.
// This function is found in the F2807x_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU __interrupts and clear all CPU __interrupt flags:
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the __interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2807x_DefaultIsr.c.
// This function is found in F2807x_PieVect.c.
//
InitPieVectTable();
//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
//
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.I2CA_INT = &i2c_int1a_isr;
EDIS; // This is needed to disable write to EALLOW protected registers
//
// Step 4. Initialize the Device Peripherals:
//
I2CA_Init();
//
// Step 5. User specific code
//
//
// Clear Counters
//
PassCount = 0;
FailCount = 0;
//
// Clear incoming message buffer
//
for (i = 0; i < I2C_MAX_BUFFER_SIZE; i++)
{
I2cMsgIn1.MsgBuffer[i] = 0x0000;
}
//
// Enable __interrupts required for this example
//
//
// Enable I2C __interrupt 1 in the PIE: Group 8 __interrupt 1
//
PieCtrlRegs.PIEIER8.bit.INTx1 = 1;
//
// Enable CPU INT8 which is connected to PIE group 8
//
IER |= M_INT8;
EINT;
for(;;)
{
//
// Write data to EEPROM section
//
//
// Check the outgoing message to see if it should be sent.
// In this example it is initialized to send with a stop bit.
//
if(I2cMsgOut1.MsgStatus == I2C_MSGSTAT_SEND_WITHSTOP)
{
Error = I2CA_WriteData(&I2cMsgOut1);
//
// If communication is correctly initiated, set msg status to busy
// and update CurrentMsgPtr for the __interrupt service routine.
// Otherwise, do nothing and try again next loop. Once message is
// initiated, the I2C __interrupts will handle the rest. Search for
// ICINTR1A_ISR in the i2c_eeprom_isr.c file.
//
if (Error == I2C_SUCCESS)
{
CurrentMsgPtr = &I2cMsgOut1;
I2cMsgOut1.MsgStatus = I2C_MSGSTAT_WRITE_BUSY;
}
}
//
// Read data from EEPROM section
//
//
// Check outgoing message status. Bypass read section if status is
// not inactive.
//
if (I2cMsgOut1.MsgStatus == I2C_MSGSTAT_INACTIVE)
{
//
// Check incoming message status.
//
if(I2cMsgIn1.MsgStatus == I2C_MSGSTAT_SEND_NOSTOP)
{
//
// EEPROM address setup portion
//
while(I2CA_ReadData(&I2cMsgIn1) != I2C_SUCCESS)
{
//
// Maybe setup an attempt counter to break an infinite while
// loop. The EEPROM will send back a NACK while it is performing
// a write operation. Even though the write communique is
// complete at this point, the EEPROM could still be busy
// programming the data. Therefore, multiple attempts are
// necessary.
//
}
//
// Update current message pointer and message status
//
CurrentMsgPtr = &I2cMsgIn1;
I2cMsgIn1.MsgStatus = I2C_MSGSTAT_SEND_NOSTOP_BUSY;
}
//
// Once message has progressed past setting up the internal address
// of the EEPROM, send a restart to read the data bytes from the
// EEPROM. Complete the communique with a stop bit. MsgStatus is
// updated in the __interrupt service routine.
//
else if(I2cMsgIn1.MsgStatus == I2C_MSGSTAT_RESTART)
{
//
// Read data portion
//
while(I2CA_ReadData(&I2cMsgIn1) != I2C_SUCCESS)
{
//
// Maybe setup an attempt counter to break an infinite while
// loop.
//
}
//
// Update current message pointer and message status
//
CurrentMsgPtr = &I2cMsgIn1;
I2cMsgIn1.MsgStatus = I2C_MSGSTAT_READ_BUSY;
}
}
}
}
//
// I2CA_Init - Initialize I2CA settings
//
void I2CA_Init(void)
{
I2caRegs.I2CSAR.all = I2C_SLAVE_ADDR; // Slave address - EEPROM control code
I2caRegs.I2CPSC.all = 6; // Prescaler - need 7-12 Mhz on module clk
I2caRegs.I2CCLKL = 10; // NOTE: must be non zero
I2caRegs.I2CCLKH = 5; // NOTE: must be non zero
I2caRegs.I2CIER.all = 0x24; // Enable SCD & ARDY __interrupts
I2caRegs.I2CMDR.all = 0x0020; // Take I2C out of reset
// Stop I2C when suspended
I2caRegs.I2CFFTX.all = 0x6000; // Enable FIFO mode and TXFIFO
I2caRegs.I2CFFRX.all = 0x2040; // Enable RXFIFO, clear RXFFINT,
return;
}
//
// I2CA_WriteData - Transmit I2CA message
//
Uint16 I2CA_WriteData(struct I2CMSG *msg)
{
Uint16 i;
//
// Wait until the STP bit is cleared from any previous master communication.
// Clearing of this bit by the module is delayed until after the SCD bit is
// set. If this bit is not checked prior to initiating a new message, the
// I2C could get confused.
//
if(I2caRegs.I2CMDR.bit.STP == 1)
{
return I2C_STP_NOT_READY_ERROR;
}
//
// Setup slave address
//
I2caRegs.I2CSAR.all = msg->SlaveAddress;
//
// Check if bus busy
//
if(I2caRegs.I2CSTR.bit.BB == 1)
{
return I2C_BUS_BUSY_ERROR;
}
//
// Setup number of bytes to send
// MsgBuffer + Address
//
I2caRegs.I2CCNT = msg->NumOfBytes+2;
//
// Setup data to send
//
I2caRegs.I2CDXR.all = msg->MemoryHighAddr;
I2caRegs.I2CDXR.all = msg->MemoryLowAddr;
for (i=0; i < msg->NumOfBytes; i++)
{
I2caRegs.I2CDXR.all = *(msg->MsgBuffer+i);
}
//
// Send start as master transmitter
//
I2caRegs.I2CMDR.all = 0x6E20;
return I2C_SUCCESS;
}
//
// I2CA_ReadData - Read I2CA Message
//
Uint16 I2CA_ReadData(struct I2CMSG *msg)
{
//
// Wait until the STP bit is cleared from any previous master communication.
// Clearing of this bit by the module is delayed until after the SCD bit is
// set. If this bit is not checked prior to initiating a new message, the
// I2C could get confused.
//
if(I2caRegs.I2CMDR.bit.STP == 1)
{
return I2C_STP_NOT_READY_ERROR;
}
I2caRegs.I2CSAR.all = msg->SlaveAddress;
if(msg->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP)
{
//
// Check if bus busy
//
if(I2caRegs.I2CSTR.bit.BB == 1)
{
return I2C_BUS_BUSY_ERROR;
}
I2caRegs.I2CCNT = 2;
I2caRegs.I2CDXR.all = msg->MemoryHighAddr;
I2caRegs.I2CDXR.all = msg->MemoryLowAddr;
I2caRegs.I2CMDR.all = 0x2620; // Send data to setup EEPROM address
}
else if(msg->MsgStatus == I2C_MSGSTAT_RESTART)
{
I2caRegs.I2CCNT = msg->NumOfBytes; // Setup how many bytes to expect
I2caRegs.I2CMDR.all = 0x2C20; // Send restart as master receiver
}
return I2C_SUCCESS;
}
//
// i2c_int1a_isr - I2CA ISR
//
__interrupt void i2c_int1a_isr(void)
{
Uint16 IntSource, i;
//
// Read __interrupt source
//
IntSource = I2caRegs.I2CISRC.all;
//
// Interrupt source = stop condition detected
//
if(IntSource == I2C_SCD_ISRC)
{
//
// If completed message was writing data, reset msg to inactive state
//
if(CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_WRITE_BUSY)
{
CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_INACTIVE;
}
else
{
//
// If a message receives a NACK during the address setup portion of
// the EEPROM read, the code further below included in the register
// access ready __interrupt source code will generate a stop
// condition. After the stop condition is received (here), set the
// message status to try again. User may want to limit the number of
// retries before generating an error.
if(CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP_BUSY)
{
CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_SEND_NOSTOP;
}
//
// If completed message was reading EEPROM data, reset msg to inactive
// state and read data from FIFO.
//
else if(CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_READ_BUSY)
{
CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_INACTIVE;
for(i=0; i < I2C_NUMBYTES; i++)
{
CurrentMsgPtr->MsgBuffer[i] = I2caRegs.I2CDRR.all;
}
{
//
// Check received data
//
for(i=0; i < I2C_NUMBYTES; i++)
{
if(I2cMsgIn1.MsgBuffer[i] == I2cMsgOut1.MsgBuffer[i])
{
PassCount++;
}
else
{
FailCount++;
}
}
}
}
}
}
//
// Interrupt source = Register Access Ready
// This __interrupt is used to determine when the EEPROM address setup
// portion of the read data communication is complete. Since no stop bit is
// commanded, this flag tells us when the message has been sent instead of
// the SCD flag. If a NACK is received, clear the NACK bit and command a
// stop. Otherwise, move on to the read data portion of the communication.
//
else if(IntSource == I2C_ARDY_ISRC)
{
if(I2caRegs.I2CSTR.bit.NACK == 1)
{
I2caRegs.I2CMDR.bit.STP = 1;
I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT;
}
else if(CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP_BUSY)
{
CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_RESTART;
}
}
else
{
//
// Generate some error due to invalid __interrupt source
//
asm(" ESTOP0");
}
//
// Enable future I2C (PIE Group 8) __interrupts
//
PieCtrlRegs.PIEACK.all = PIEACK_GROUP8;
}
//
// pass - Halt debugger and signify pass
//
void pass()
{
asm(" ESTOP0");
for(;;);
}
//
// fail - Halt debugger and signify fail
//
void fail()
{
asm(" ESTOP0");
for(;;);
}
//
// End of file
//