This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Flowting GPIOs

Part Number: TMS320F28379D


Hello,
customer has open GPIOs in his design which are set to input. Is this allowed? Can this have an influence on the ADC measurement?

Regards, Holger

  • Holger,

    there are 3 acceptable configurations for unused GPIOs.

    1. Input mode with internal pullup enabled
    2. Input mode with external pullup or pulldown resistor
    3. Output mode with internal pullup disabled

    As long as the unused GPIO is at a steady state and not "wiggling" then it will not affect the ADC measurement.

    Regards,
    Cody