Other Parts Discussed in Thread: SFRA, CONTROLSUITE, POWERSUITE
Hello,
I am currently working with the Vienna Rectifier-Based, Three-Phased PFC and have been having some issues with the initial testing. I have been following the users guide and am currently following the steps for the INCR_BUILD 1: Open Loop (6.4.1). I am using a 3 Phase Delta supply as my power source so I have no neutral connection, I believe this is my issue. In the setup it says to connect the neutral to the DC mid point in the output bus, I cannot make this connection since I have no neutral from my supply. When I increase my input to 208 L-L my input current waveforms do not look like the ones shown in Figure 23, they look more like the ones shown in Figure 46. Figure 46 is from the INCR_BUILD 4 section where it instructs you to remove the neutral connection from the DC mid point on the output bus.
So my question is, since I don't have the neutral connection is that why my current waveforms look like Figure 46 instead of Figure 23? And is it possible to work through Build 1 to 3 without the connection?
Best Regards,
Luke