This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28377S: Error while trying to flash the code using XDS100v2 debugger

Part Number: TMS320F28377S


Tool/software: TI C/C++ Compiler

Hi,

I am using f28377s lunchpad. I have been working on the board since last month. recently i am facing the issue while trying to flash the code using CCS studio. It shows the error as below.I tried reseting the board but the error still persists. I checked with the other f28377s launch-XLboard, there is no issue in CCS or in the target configuration.Can anyone please help me with this issue??

  • Even the Jtag Integration test using Test connection in target configuration utility has failed. Can anybody address this issue??? A quick reply is most appreciated.
    thank you
  • Chandana,

    It seems CCS can not find the JTAG. Make sure that JTAG(or board) is connected to your PC correctly.

    1) Try to change usb port and cable.
    2) There must be some leds turning on when you connect usb cable to board. Make sure that they are ON, when you connect usb cable. If they are not ON, you probably have an HW problem.
    3) Uninstall and reinstall JTAG drivers. Make sure that JTAG is visible in the "Device Manager" of Windows.

    Regards,
    Hakan
  • Thanks for the reply Hakan.

    There was  a problem with JP1 jumper. so the controller section was not powered.I was able to solve the issue.